Feedback_Kv

Feedback_Kv

Address: 10242 (2802H)
Type: Unsigned32
Access: Read/Write
Unit: --
Range: Unsigned32
Default Value: 8000
Store Supported: Yes
Description:

This value is used for Feedback feature and define the velocity Gain of PID’s regulator. The value has to be adjust to keep the Feedback_Velocity_Position_Error inside the tolerance of application. Pay attention that a not coherent value (big value) can introduce motor’s vibration.

Notes: See Closed Loop Modality for details.